Pin Packages

pin-packages-group-12462

PIN PACKAGES FOR ACCURATE POSITIONING OF SHEET METAL & WORK PARTS

DESTACO Pin Locator Clamps are primarily used in the automotive industry as a precision locating device to locate sheet metal parts for weld assembly. The pin locator units can have various attachments that are used for part location. One attachment is an NAAMS pin that is inserted into the arm that extends and retracts from the unit. This pin locates a datum hole in the part to constrain the part.

Markets: AerospaceAutomotiveFood and PackagingConsumer Goods, Industrial

Applications: Fixturing and Testing, Welding, CNC Machining

Unit View:
compact-size
precision
performance
interchangeable
Back to Top