DESTACO Introduces Front-Mount-Base Manual Clamp Models

New design offers four new options for horizontal or vertical handle action

Mar 29,2022-Mar 30,2030 | Tags: Press Releases & News Articles - Global
Destaco News & Events Image

Oberursel, Hesse (March 30, 2022) – DESTACO is pleased to announce that it is expanding the range of its horizontal and vertical toggle-lock Manual Clamp product line with the introduction of a front-mount-base model. The compact, space-saving front-mount base is designed to offer users additional flexibility in their workholding applications.

“The clamp’s vertical foot provides for higher user flexibility. The position of the base leads to significant reduction in interfering contours,” explained Nina Wolleb, Application Engineering Manager, Europe for DESTACO.

The front-mount option is available for inclusion on a total of four manual clamps that can be used with both vertical and horizontal handle action. The two vertical operating models – 2002-UF and 2007-UF – provide enlarged space for manual operations and increased safety. The horizontal versions – models 225-UF and 235-UF – have a flat design that creates space for larger hand clearance, which improves operational safety.

The new models use the same connection-hole pattern as existing models, along with the same spindles, pin holders and bolt retainers. All models have hardened bushings at key pivot points and the design does not interfere with the mounting connections.

To learn more about DESTACO or any of its high-performance automation, workholding or remote-handling solutions, please visit destaco.com or call (888) DESTACO (888-337-8226).

About DESTACO

DESTACO, a Dover Corporation company, is a global leader in the design and manufacture of high-performance automation, workholding and remote-handling solutions. The company serves customers in a variety of end-markets, including the automotive, life sciences, consumer packaged goods, aerospace, industrial and nuclear sectors.

Built on a legacy of more than 100 years, DESTACO offers a comprehensive portfolio of products designed to engineer precise movement, placement and control solutions that drive productivity and uptime for manufacturers around the world. The DESTACO family of products consists of industry-leading brands such as DESTACO Manual Clamps, Power Clamps, and End Effectors; Camco and Ferguson Indexers; Robohand Grippers; and CRL Manipulators and Transfer Ports.

DESTACO is based in Auburn Hills, Michigan, U.S.A. The company has more than 800 employees with 13 locations, in 9 countries, across the Americas, Europe and Asia. More information is available at destaco.com.

DESTACO is part of Dover Corporation, a diversified global manufacturer and solutions provider with annual revenue of approximately $8 billion. We deliver innovative equipment and components, consumable supplies, aftermarket parts, software and digital solutions, and support services through five operating segments: Engineered Products, Clean Energy & Fueling, Imaging & Identification, Pumps & Process Solutions and Climate & Sustainability Technologies. Dover combines global scale with operational agility to lead the markets we serve. Recognized for our entrepreneurial approach for more than 65 years, our team of more than 25,000 employees takes an ownership mindset, collaborating with customers to redefine what's possible. Headquartered in Downers Grove, Illinois, Dover trades on the New York Stock Exchange under "DOV." Additional information is available at dovercorporation.com.   

Back to Top